I am working on the i.MX93EVK. I am trying to switch the board to a low-power LD mode. NXP application note AN13917 details different power modes (e.g., OD, ND, LD) and how to switch between them. However, not all of the commands work. I can get into OD and ND modes, but I cannot get into the low-power LD modes. If I try to switch to LD mode, I get an invalid argument error (see bash output below). I tried booting both NXP Linux L6.6.3 and L6.1.55. Is there something I am missing?
root@imx93evk:~# echo 1 > /sys/devices/platform/imx93-lpm/mode
[ 2560.222108] System switching to ND mode...root@imx93evk:~# echo 0 > /sys/devices/platform/imx93-lpm/mode[ 2620.258231] System switching to OD mode...root@imx93evk:~# echo 2 > /sys/devices/platform/imx93-lpm/mode-sh: echo: write error: Invalid argumentroot@imx93evk:~# echo 3 > /sys/devices/platform/imx93-lpm/mode-sh: echo: write error: Invalid argument
解決済! 解決策の投稿を見る。
The problem was that I needed to boot with a special DTB file: "imx93-11x11-evk-ld.dtb". In U-Boot, I ran "setenv fdtfile imx93-11x11-evk-ld.dtb" followed by "boot". This fixed the issue for me.
The problem was that I needed to boot with a special DTB file: "imx93-11x11-evk-ld.dtb". In U-Boot, I ran "setenv fdtfile imx93-11x11-evk-ld.dtb" followed by "boot". This fixed the issue for me.