Hi,
I got some Chinese tablet that runs Debian, and it has NXP i.MX 8M Mini 4xCortex-A53 1.6Ghz processor.
uname -a output:
Linux imx8 4.14.98-2.3.0+ #1 SMP PREEMPT Mon Nov 8 02:36:19 UTC 2021 aarch64 GNU/Linux
https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8-GStreamer-User-Guide/ta-p/1098942 guide states that "somewhere" where are various gstreamer plugins for encoding/decoding video on IMX processors, but not really sure where do I get them from?
Will I be able to build these plugins for (within?) Debian system?
Thanks!
Solved! Go to Solution.
It seems I have to use https://github.com/Freescale/gstreamer-imx , with dependencies https://github.com/Freescale/libimxvpuapi and https://github.com/Freescale/libimxdmabuffer . I had to use board toolchain provided by device developers so that imx kernel headers where available, together with some libraries like libg2d, etc.
After building it all, I had to use LD_LIBRARY_PATH, GST_PLUGINS env. variables to help application to find all required libraries and newly built gstreamer plugins, and it works by specifying custom GStreamer pipeline:
rtspsrc location=rtsp://user:pass@host:554/cam/realmonitor?channel=1&subtype=0&unicast=true protocols=udp latency=100 ! rtph264depay ! h264parse ! imxvpudec_h264 ! qtvideosink
Decoding performance is much better, though system still lacks OpenGL HW acceleration, so application is still laggy, but that's other issue...
It seems I have to use https://github.com/Freescale/gstreamer-imx , with dependencies https://github.com/Freescale/libimxvpuapi and https://github.com/Freescale/libimxdmabuffer . I had to use board toolchain provided by device developers so that imx kernel headers where available, together with some libraries like libg2d, etc.
After building it all, I had to use LD_LIBRARY_PATH, GST_PLUGINS env. variables to help application to find all required libraries and newly built gstreamer plugins, and it works by specifying custom GStreamer pipeline:
rtspsrc location=rtsp://user:pass@host:554/cam/realmonitor?channel=1&subtype=0&unicast=true protocols=udp latency=100 ! rtph264depay ! h264parse ! imxvpudec_h264 ! qtvideosink
Decoding performance is much better, though system still lacks OpenGL HW acceleration, so application is still laggy, but that's other issue...