Hello!
I am currently using 2 i.MX 8mp evaluation kit boards and 1 LS1021ATSN switch.
And for a simple test, I made a small network using them as below.
h1 <eth0> - <eth2> switch <eth1> - <eth1> h2
The static IP addresses I gave for each of the interfaces are as below.
h1 eth0 : 192.168.2.101
switch eth2 : 192.168.2.202
switch eth1 : 192.168.2.10
h2 eth1 : 192.168.2.5
I did ping tests for the links between h2 - switch and h1 - switch. And for the link between h2 and the switch, the ping works well. However, for the link between h1 and the switch, the ping fails.
I cannot find out the reason why it doesn’t work. So, can you please help me?
Thanks all, in advance.
Thank you!
Hello,
I can help you troubleshoot the ping failure between h1 and the switch in your network setup. Here are some steps you can follow:
1. Double-Check Cable Connections:
2. Verify IP Address Configuration:
3. Check Switch Configuration (if applicable):
By following these steps systematically, you should be able to identify the cause of the ping failure and establish a successful connection between h1 and the switch.