Mar 13, 2020: imx_builder_03122020.tgz --- change the i.MX8MN configuration.
Dec 11, 2019: imx_builder_12112019.tgz --- add support L4.19.35_1.1.0
August 28, 2019: imx_builder_08282019.tgz --- add i.MX8MM
July 03, 2019: imx_builder_07032019.tgz --- add i.MX8QM: build_i.MX8
Feb 26, 2020: imx_builder_02262020 --- add i.MX8MN, add spl m4 for build_i.MX8, build_i.MX8X with L4.14.98_2.0.0_ga, L4.14.98_2.2.0, L4.19.35_1.1.0
imx_builder_02262020:
imx_builder is a set of Makefile for build u-boot, Linux kernel, atf, scfw, imx-mkimage. You can call it standalone build.
here is the step to try it.
You can use -n for make to get the detail build steps.
ex: make atf -n
make linux.Image -n
L4.14.78_ga as example:
1. Untar imx_builder_02282019.tgz
2. Read the Standalone_Build_Preparation.pdf inside to prepare the bsp.
3. Prepare the toolchains(populate_sdk from yocto, get from linaro, get from buildroot, etc.)
4. Prepare scfw toolchains following the SCFW Porting Kit.
5. Follow the Standalone_Build_Preparation.pdf to check if the Build Structure is correct.
L4.14.78_1.0.0_ga as example.
Prepare rel_imx_4.14.78_1.0.0_ga in REL
Make symbol link to REL/rel_imx_4.14.78_1.0.0_ga
Make symbol link to build_i.MX8X
imx_builder/
|-- atf -> bsp/imx-atf
|-- bsp -> REL/rel_imx_4.14.78_1.0.0_ga
|-- build -> build_i.MX8X
|-- build_i.MX6
|-- build_i.MX8M
|-- build_i.MX8X
| |-- Makefile -> Makefile.4.14.78_ga
| |-- Makefile.4.14.78_ga
| |-- README
| |-- SETTINGS_4.14.78_1.0.0_ga.MK
| |-- SETTINGS.MK -> SETTINGS_4.14.78_1.0.0_ga.MK
| `-- VERSION.MK
|-- dts -> linux/arch/arm/boot/dts
|-- imx-mkimage -> bsp/imx-mkimage
|-- linux -> bsp/linux-imx
|-- Makefile -> build/Makefile
|-- Others
|-- out
|-- README -> build/README
|-- REL
| `-- rel_imx_4.14.78_1.0.0_ga
| |-- firmware-imx-8.0.bin
| |-- imx-atf
| |-- imx-mkimage
| |-- imx-sc-firmware-1.1.bin(optional)
| |-- imx-scfw-porting-kit-1.1.tar.gz
| |-- linux-imx
| `-- uboot-imx
|-- scfw -> bsp/scfw
|-- SETTINGS.MK -> build/SETTINGS.MK
|-- Standalone_Build_Preparation.pdf
|-- toolchains
| `-- scfw
| `-- gcc-arm-none-eabi-6-2017-q2-update
|-- u-boot -> bsp/uboot-imx
`-- VERSION.MK -> build/VERSION.MK
imx_builder_03122020.tgz, and building the i.MX 8MM, the Makefile has target defined for rootfs.tar, however missing ${FS_TAR_SCRIPT} defined in SETTINGS.MK:
FS_DIR=${PWD}/fs
FS_TAR_DIR=${FS_DIR}/tar
FS_TAR_SCRIPT=${FS_TAR_DIR}/rootfs.tar.gz.sh
Can the full FS_DIR and scripts for all sub directories be provided in imx_builder?
Missing:
fs/tar
fs/ubi
fs/cpio
At the very initial version of imx_builder, I just add a very small rootfs for test purpose.
And I decide not to support rootfs any more. But I didn't remove the rules.
Acuatully, I made the small test rootfs by buildroot.
Hi BiyongSUN, thanks for the update.
Here is script (getSw.sh) to populate the bsp directory. Using release rel_imx_5.4.24_2.1.0, for firmware-imx, the i.MX_Linux_Release_Notes.pdf had the version (8.8) for this release. To use other Linux releases, update the TAG and FWR variable for the versions needed.
#!/bin/bash
TAG="rel_imx_5.4.24_2.1.0"
FWR="8.8"
CAF="https://source.codeaurora.org/external/imx"
MAD="wget https://www.nxp.com/lgfiles/NMG/MAD/YOCTO"
wget ${MAD}/firmware-imx-${FWR}.bin
for repo in linux-imx uboot-imx imx-atf imx-mkimage; do
git clone ${CAF}/${repo} -b ${TAG};
done
Thanks a lot for your script.
I have a similar one, which remove the .git in linunx-imx, uboot-imx to make the bsp small.
I think it not part of the imx_builder so far.
And my initial thought is for customers to understand the standalone build. and easy to see the single steps, which is a little bit hard to read in Yocto.
The imx_builder is for a professional user like you. You can add any new feature like preparing bsp.
Thanks a lot for your interesting in my imx_builder.