Video - Genesi's Hard Float optimizations speeds up Linux performance up to 300% on ARM Laptops

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Video - Genesi's Hard Float optimizations speeds up Linux performance up to 300% on ARM Laptops

Video - Genesi's Hard Float optimizations speeds up Linux performance up to 300% on ARM Laptops

http://www.youtube.com/watch?v=qWUd4TAEqTM&feature=player_embedded

 

Uploaded by Charbax on Jun 20, 2011

Konstantinos Margaritis is a Senior Software Engineer at San Antonio based Genesi, he talks about how Genesi is pushing Linaro forward to recompile all the apps and everything around Linux to use hard float, to re-optimize floating point applications on ARM Powered Desktop/Laptop designs. Watch this video interview to find out how Genesi is doing these software optimizations on Debian for the i.MX51 and i.MX53 platforms in their ARM Powered Smartbook designs. How soon are ARM Powered laptops going to have enough performance optimizations in them to demonstrate that ARM is fast enough to power Desktop/Laptop designs so that every consumer can be satisfied with the performance?

Category:

Science & Technology

License:

Standard YouTube License

 

标签 (1)
标记 (1)
无评分
版本历史
最后更新:
‎08-23-2012 04:08 PM
更新人: