Video - Genesi's Hard Float optimizations speeds up Linux performance up to 300% on ARM Laptops

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Video - Genesi's Hard Float optimizations speeds up Linux performance up to 300% on ARM Laptops

Video - Genesi's Hard Float optimizations speeds up Linux performance up to 300% on ARM Laptops

http://www.youtube.com/watch?v=qWUd4TAEqTM&feature=player_embedded

 

Uploaded by Charbax on Jun 20, 2011

Konstantinos Margaritis is a Senior Software Engineer at San Antonio based Genesi, he talks about how Genesi is pushing Linaro forward to recompile all the apps and everything around Linux to use hard float, to re-optimize floating point applications on ARM Powered Desktop/Laptop designs. Watch this video interview to find out how Genesi is doing these software optimizations on Debian for the i.MX51 and i.MX53 platforms in their ARM Powered Smartbook designs. How soon are ARM Powered laptops going to have enough performance optimizations in them to demonstrate that ARM is fast enough to power Desktop/Laptop designs so that every consumer can be satisfied with the performance?

Category:

Science & Technology

License:

Standard YouTube License

 

ラベル(1)
タグ(1)
評価なし
バージョン履歴
最終更新日:
‎08-23-2012 04:08 PM
更新者: