lwip_tcpecho client

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

lwip_tcpecho client

1,033件の閲覧回数
li-chinwang
Contributor II

i.MX RT 1050 has lwip example test lwip_tcpecho.

i.MX RT1050  EVK play role of tcp sever.

Do you have example like this but playing role of tcp_client?

ラベル(1)
タグ(2)
0 件の賞賛
1 返信

789件の閲覧回数
CarlosCasillas
NXP Employee
NXP Employee

Hi Wang,

There is not available a specific “tcp_client” example, just those available on the “lwip_examples”.

According with the “MCUXpresso SDK Release Notes Supporting EVKB-IMXRT1050” document, the current version of lwIP is based on lwIP 2.0.3, and referring to lwIP Overview webpage (link below), you could verify the supported features:

http://www.nongnu.org/lwip/2_0_x/index.html


Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛