RT1050 connect with two camera

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT1050 connect with two camera

1,224 Views
captain_huang
Contributor I

In the i.MX RT1050 Processor Reference Manual  :

pastedImage_2.png

it said the rt1050 support to connect with two camera sensors. so anybody who can tell me hao to use this function. i need to connect with two camera in my application.

tks!

Labels (1)
0 Kudos
Reply
1 Reply

1,086 Views
igorpadykov
NXP Employee
NXP Employee

Hi chao

one can look at AN12103 and its software example to modify sources

for receiving data from two cameras

AN12103 Developing a simple UVC device based on i.MX RT1050

https://www.nxp.com/docs/en/application-note/AN12103.pdf 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply