i.mx rt1050 booting from LPSPI

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.mx rt1050 booting from LPSPI

Jump to solution
2,547 Views
christiangradl
Contributor III

What are the exact bootmode/pins settings for booting via LPSPI?

in the TRM table 8-8 there is no entry about this.

Above there stands

   The chip supports these boot flash devices

       Serial NOR/EEPROM boot via LPSPI

Labels (1)
1 Solution
2,207 Views
christiangradl
Contributor III

OK, thanx, that info helps.

View solution in original post

0 Kudos
Reply
4 Replies
2,207 Views
igorpadykov
NXP Employee
NXP Employee

Hi Christian

pinmux settings are given in Table 8-1. ROM Bootloader Peripheral PinMux
i.MX RT1050 Processor Reference Manual

Boot mode only using fuse mode as shows Table 8-35 (there is no GPIO override mode),
fuse selections are given in Table 5-9. Fusemap Descriptions i.MX RT1050 Processor
Reference Manual
https://www.nxp.com/docs/en/reference-manual/IMXRT1050RM.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
2,207 Views
christiangradl
Contributor III

Hi

in table 5-9 there is no definition for booting woth LPSPI. Register 0x450[7:0]???

I can select the LPSPI chipselect register 0x6D0, but how can i select the boot device for LPSPI,

as described in chapter 8-2

    The boot ROM supports these boot devices:
   • Serial NOR Flash via FlexSPI
   • Serial NAND Flash via FlexSPI
   • Parallel NOR Flash via SEMC
   • RAWNAND Flash via SEMC
   • SD/MMC
   • SPI NOR/EEPROM via LPSPI

0 Kudos
Reply
2,207 Views
igorpadykov
NXP Employee
NXP Employee

boot ROM uses it as recovery device using one of the LPSPI ports,

please check description in sect.8.10 Recovery devices

Best regards
igor

0 Kudos
Reply
2,208 Views
christiangradl
Contributor III

OK, thanx, that info helps.

0 Kudos
Reply