i.MX RT600 + murata Wi-Fi Module supports WHD driver or not

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX RT600 + murata Wi-Fi Module supports WHD driver or not

844件の閲覧回数
Sachin2
Contributor I

Hi There,

i.MX RT600 + murata Wi-Fi Module supports WHD driver or not?

I'm using SDK_2_10_1_EVK-MIMXRT685 and MCUXpressoIDE_11.4.1_6260

Thanks,

ラベル(1)
0 件の賞賛
1 返信

830件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @Sachin2 

To the SDK_2_10_1_EVK-MIMXRT685, I find the wifi for the murata wifi module driver is removed, it just contains the nxp wifi module.

- One of the following Wi-Fi modules:
- Panasonic PAN9026 SDIO ADAPTER
- AzureWave AW-NM191NF-uSD + uSD to SD adapter
- AzureWave AW-AM457-uSD + uSD to SD adapter
- AzureWave AW-CM358-uSD + uSD to SD adapter

Even to the old SDK SDK_2.9.0_EVK-MIMXRT685 which contains the murrata module, i search the project, and didn't find the WHD driver, so maybe you need to port it by yourself, and refer to the cypress porting information:

https://infineon.github.io/wifi-host-driver/html/index.html

More details about the murrata, please contact cypress, thanks.

Best Regards,

Kerry

 

0 件の賞賛