i.MX RT600 + murata Wi-Fi Module supports WHD driver or not

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX RT600 + murata Wi-Fi Module supports WHD driver or not

828 Views
Sachin2
Contributor I

Hi There,

i.MX RT600 + murata Wi-Fi Module supports WHD driver or not?

I'm using SDK_2_10_1_EVK-MIMXRT685 and MCUXpressoIDE_11.4.1_6260

Thanks,

Labels (1)
0 Kudos
1 Reply

814 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @Sachin2 

To the SDK_2_10_1_EVK-MIMXRT685, I find the wifi for the murata wifi module driver is removed, it just contains the nxp wifi module.

- One of the following Wi-Fi modules:
- Panasonic PAN9026 SDIO ADAPTER
- AzureWave AW-NM191NF-uSD + uSD to SD adapter
- AzureWave AW-AM457-uSD + uSD to SD adapter
- AzureWave AW-CM358-uSD + uSD to SD adapter

Even to the old SDK SDK_2.9.0_EVK-MIMXRT685 which contains the murrata module, i search the project, and didn't find the WHD driver, so maybe you need to port it by yourself, and refer to the cypress porting information:

https://infineon.github.io/wifi-host-driver/html/index.html

More details about the murrata, please contact cypress, thanks.

Best Regards,

Kerry

 

0 Kudos