i.MX RT1170 CAN bootloder

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX RT1170 CAN bootloder

886件の閲覧回数
scarletlee
Contributor III

Hi,

Have a CAN bootloader for i.MX RT1170?

I tried to search bootloader information but only USB bootloader.

Thanks.

タグ(1)
0 件の賞賛
3 返答(返信)

876件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Have a CAN bootloader for i.MX RT1170?
-- The Serial Boot doesn't support other peripherals except for the UART and USB, so it needs the developers to implement a secondary bootloader that supports the CAN interface.

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛

862件の閲覧回数
scarletlee
Contributor III

Hi Jeremy,

 

Thanks for your reply.

So...your mean is CANBUS bootloader must developer by myself or maybe NXP can provide an example?

 

Best Regards,

Scarlet

0 件の賞賛

857件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thanks for your reply.
1)So...your mean is CANBUS bootloader must developer by myself or maybe NXP can provide an example?
-- As I know, there's no similar demo now for you to refer to.

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛