i.MX RT1170 CAN bootloder

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX RT1170 CAN bootloder

1,230 Views
scarletlee
Contributor III

Hi,

Have a CAN bootloader for i.MX RT1170?

I tried to search bootloader information but only USB bootloader.

Thanks.

Tags (1)
0 Kudos
Reply
3 Replies

1,220 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Have a CAN bootloader for i.MX RT1170?
-- The Serial Boot doesn't support other peripherals except for the UART and USB, so it needs the developers to implement a secondary bootloader that supports the CAN interface.

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

1,206 Views
scarletlee
Contributor III

Hi Jeremy,

 

Thanks for your reply.

So...your mean is CANBUS bootloader must developer by myself or maybe NXP can provide an example?

 

Best Regards,

Scarlet

0 Kudos
Reply

1,201 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thanks for your reply.
1)So...your mean is CANBUS bootloader must developer by myself or maybe NXP can provide an example?
-- As I know, there's no similar demo now for you to refer to.

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply