i.MX RT list of supported HyperFlash devices (octal flash)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX RT list of supported HyperFlash devices (octal flash)

Jump to solution
1,834 Views
nickwallis
Senior Contributor I

Hi,

Please can you share a list of i.MX RT supported HyperFlash devices (octal flash)?

thanks

-Nick

0 Kudos
1 Solution
1,817 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thanks for your reply.
1) Which document is this table from?
-- The table is from the AN12107.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
6 Replies
1,470 Views
tfborth
Contributor I

Hi, is MX66UM1G45G also compatible? I'm looking for a 1Gb memory but it's seems that there is no one avaliable at Table 9...

0 Kudos
1,446 Views
jeremyzhou
NXP Employee
NXP Employee

Hi @tfborth ,

1) is MX66UM1G45G also compatible?

-- Yes.

BR,

Jeremy

1,430 Views
tfborth
Contributor I

Hi, thanks!

0 Kudos
1,828 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Please can you share a list of i.MX RT supported HyperFlash devices (octal flash)?
-- Please refer to the below figure, moreover, it's available to select the compatible octal flash for design.

jeremyzhou_0-1645521365934.png

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
1,824 Views
nickwallis
Senior Contributor I

thanks @jeremyzhou 

Which document is this table from?

I looked in AN12107 and whilst table 9 is referenced in the revision history, there is no table 9 in the actual document?

-Nick

0 Kudos
1,818 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thanks for your reply.
1) Which document is this table from?
-- The table is from the AN12107.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos