.dts support for RT in Pins for iMX tool

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

.dts support for RT in Pins for iMX tool

645件の閲覧回数
dav1
Contributor V

Dear NXP,

Would be awesome if you could add .dts output (and even kconfig) to the Pins tool for the i.MX RT series.

This is very useful when designing with RT's using the Zephyr project RTOS.

Thanks 

ラベル(2)
0 件の賞賛
1 返信

558件の閲覧回数
victorjimenez
NXP TechSupport
NXP TechSupport

Hello, 

Thanks for your feedback! I will pass the information to the corresponding team. 


Have a great day,
Victor

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛