Why would a DSB instruction never complete?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Why would a DSB instruction never complete?

5,443 Views
chriscowdery
Contributor V

Hi All,

MIMXRT1021DAF5A, IAR compiler, FreeRTOS, code in Serial Flash (SQPI)

 I have a DSB instruction that never completes. This causes a processor 'lockup'. This is the sequence of events:

1. Code executing normally

2. SysTick interrupt occurs.

3. System 'stops'. (I do not know why it stops - I guess the pipeline has just fetched the DSB instruction)

4. Using J-Link Commander, I 'halt' and read register contents. I can confirm PC = first instruction of SysTick handler. Stack & registers OK, and consistent.

5. Using J-Link Commander, I 'single step' :

6. PUSH {R7,LR} - OK

7. MOVS R0,#32 - OK

8. MSR BASEPRI,R0 - OK

9. DSB #15 - Any J-Link Commander command after this reports 'CPU is not halted!'. Trying to 'halt' the CPU says 'WARNING: CPU could not be halted'

I think this means the DSB instruction never completed. I think the CPU is waiting for an input to allow DSB to complete which never comes.

Why would a DSB instruction never complete?

Thanks,

Chris.

Labels (1)
31 Replies

1,595 Views
chriscowdery
Contributor V

Hi Kerry,

 Are you saying that all memory should be changed to DEVICE_MEMORY or STRONGLY_ORDERED? This will stop the prefetch?

But it also stops the Cache right?

Thanks,

Chris.

0 Kudos

1,595 Views
chriscowdery
Contributor V

For example

LDR   R0,#0

LDR   R1,=0x40000000   ;No memory at this address

TST   R0,#0

BEQ   jump   ;will always branch

LDR   R0,[R1]  ; will attempt to read an invalid memory location if speculatively executed, will cause a fault?

.jump

Will that cause a fault?

How can I stop it causing a fault?

Is the only fix to disable speculative fetching?

Chris.

0 Kudos

1,595 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Chris Cowdery

   Can you simplify your question, and reproduce your issue with the SDK and the NXP MIMXRT1020EVK board?

  Take an example, when you use some of your asm examples, then enter the fault or the lockup issue, and let me reproduce that issue and check more details about it, it may be more visually discuss your problems. Even I meet some issues after reproducing your issue, I also can check it with our internal side, otherwise, just some asm code piece, I am also a little confused about the detail speculate result, sorry about it.

Best Regards,

Kerry

1,595 Views
chriscowdery
Contributor V

Hi Kerry,

 I think I have fixed it. I found the MPU was incorrectly configured. I had taken a reference project for the EVK, but now I understand it better, I found the setup was wrong.

I have no idea why that would cause instructions to not complete in the Debugger though!!

But my system appears stable now... I hope!

Chris.

0 Kudos

1,595 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Chris Cowdery,

  Do you mean the SDK MPU configuration is incorrect, or your own project?

  Could you please also share your detail MPU configuration and the detail root point which will cause your issues?

  Thanks a lot for your contribution.

Best Regards,

Kerry

1,595 Views
chriscowdery
Contributor V

Hi Kerry,

 I mean all the Example Projects in the SDK that I have looked at are wrong. Here is one from evkmimx1020->rtos_examples->freertos_generic.

I think I used this as my base project.

board.c:

/* MPU configuration. */
void BOARD_ConfigMPU(void)
{
    /* Disable I cache and D cache */
    if (SCB_CCR_IC_Msk == (SCB_CCR_IC_Msk & SCB->CCR)) {
        SCB_DisableICache();
    }
    if (SCB_CCR_DC_Msk == (SCB_CCR_DC_Msk & SCB->CCR)) {
        SCB_DisableDCache();
    }

    /* Disable MPU */
    ARM_MPU_Disable();

    /* Region 0 setting */
    MPU->RBAR = ARM_MPU_RBAR(0, 0xC0000000U);
    MPU->RASR = ARM_MPU_RASR(0, ARM_MPU_AP_FULL, 2, 0, 0, 0, 0, ARM_MPU_REGION_SIZE_512MB);

    /* Region 1 setting */
    MPU->RBAR = ARM_MPU_RBAR(1, 0x80000000U);
    MPU->RASR = ARM_MPU_RASR(0, ARM_MPU_AP_FULL, 2, 0, 0, 0, 0, ARM_MPU_REGION_SIZE_1GB);

    /* Region 2 setting */
#if defined(XIP_EXTERNAL_FLASH)
    MPU->RBAR = ARM_MPU_RBAR(2, 0x60000000U);
    MPU->RASR = ARM_MPU_RASR(0, ARM_MPU_AP_FULL, 0, 0, 1, 1, 0, ARM_MPU_REGION_SIZE_512MB);
#else
    MPU->RBAR = ARM_MPU_RBAR(2, 0x60000000U);
    MPU->RASR = ARM_MPU_RASR(0, ARM_MPU_AP_FULL, 2, 0, 0, 0, 0, ARM_MPU_REGION_SIZE_512MB);
#endif

    /* Region 3 setting */
    MPU->RBAR = ARM_MPU_RBAR(3, 0x00000000U);
    MPU->RASR = ARM_MPU_RASR(0, ARM_MPU_AP_FULL, 2, 0, 0, 0, 0, ARM_MPU_REGION_SIZE_1GB);
    
    /* Region 4 setting */
    MPU->RBAR = ARM_MPU_RBAR(4, 0x00000000U);
    MPU->RASR = ARM_MPU_RASR(0, ARM_MPU_AP_FULL, 0, 0, 1, 1, 0, ARM_MPU_REGION_SIZE_128KB);

    /* Region 5 setting */
    MPU->RBAR = ARM_MPU_RBAR(5, 0x20000000U);
    MPU->RASR = ARM_MPU_RASR(0, ARM_MPU_AP_FULL, 0, 0, 1, 1, 0, ARM_MPU_REGION_SIZE_128KB);

    /* Region 6 setting */
    MPU->RBAR = ARM_MPU_RBAR(6, 0x20200000U);
    MPU->RASR = ARM_MPU_RASR(0, ARM_MPU_AP_FULL, 0, 0, 1, 1, 0, ARM_MPU_REGION_SIZE_256KB);

    /* The define sets the cacheable memory to shareable,
     * this suggestion is referred from chapter 2.2.1 Memory regions,
     * types and attributes in Cortex-M7 Devices, Generic User Guide */
#if defined(SDRAM_IS_SHAREABLE)
    /* Region 7 setting, set whole SDRAM can be accessed by cache */
    MPU->RBAR = ARM_MPU_RBAR(7, 0x80000000U);
    MPU->RASR = ARM_MPU_RASR(0, ARM_MPU_AP_FULL, 0, 1, 1, 1, 0, ARM_MPU_REGION_SIZE_32MB);
#else
    /* Region 7 setting, set whole SDRAM can be accessed by cache */
    MPU->RBAR = ARM_MPU_RBAR(7, 0x80000000U);
    MPU->RASR = ARM_MPU_RASR(0, ARM_MPU_AP_FULL, 0, 0, 1, 1, 0, ARM_MPU_REGION_SIZE_32MB);
#endif

    /* Region 8 setting, set last 2MB of SDRAM can't be accessed by cache, glocal variables which are not expected to be accessed by cache can be put here */
    MPU->RBAR = ARM_MPU_RBAR(8, 0x81E00000U);
    MPU->RASR = ARM_MPU_RASR(0, ARM_MPU_AP_FULL, 1, 0, 0, 0, 0, ARM_MPU_REGION_SIZE_2MB);   

    /* Enable MPU */
    ARM_MPU_Enable(MPU_CTRL_PRIVDEFENA_Msk);
    
    /* Enable I cache and D cache */
    SCB_EnableDCache();
    SCB_EnableICache();
}

You can see that the memory sizes for ITCM, DTCM and OCRAM are incorrect.

I found a few other things that I thought were incorrect.

This is my version:

/* MPU configuration. */
void BOARD_ConfigMPU(void)
{
    /* Disable I cache and D cache */
    if (SCB_CCR_IC_Msk == (SCB_CCR_IC_Msk & SCB->CCR)) {
        SCB_DisableICache();
    }
    if (SCB_CCR_DC_Msk == (SCB_CCR_DC_Msk & SCB->CCR)) {
        SCB_DisableDCache();
    }

    /* Disable MPU */
    ARM_MPU_Disable();

    // Document AN12042 'Using the i.MXRT L1 Cache'
    // page 5 gives the default configuration, which is overlaid with this one
    // where differences exist (i.e. if a region is not specified below,
    // it retains it's default configuration)
    // ARM_MPU_RASR(DisableExec, AccessPermission, TypeExtField, IsShareable, \
    // IsCacheable, IsBufferable, SubRegionDisable, Size)    
    
    // 0x80000000-0xDFFFFFFF is external memory like SDRAM etc. Not used.
    /* Region 0 setting */ // give external memories no access (1.5Gb total 0x80000000-0xdfffffff)
    MPU->RBAR = ARM_MPU_RBAR(0, 0xC0000000U);
    MPU->RASR = ARM_MPU_RASR(0, ARM_MPU_AP_NONE, 0, 0, 0, 0, 0, ARM_MPU_REGION_SIZE_512MB);

    /* Region 1 setting */ // give external memories no access
    MPU->RBAR = ARM_MPU_RBAR(1, 0x80000000U);
    MPU->RASR = ARM_MPU_RASR(0, ARM_MPU_AP_NONE, 0, 0, 0, 0, 0, ARM_MPU_REGION_SIZE_1GB);

    /* Region 2 setting */
    // External flash at 0x60000000-0x7fffffff. Cacheable and executable.
    MPU->RBAR = ARM_MPU_RBAR(2, 0x60000000U);
    MPU->RASR = ARM_MPU_RASR(0, ARM_MPU_AP_FULL, 0, 0, 1, 1, 0, ARM_MPU_REGION_SIZE_512MB);

    /* Region 3 setting */
    // This is all of RAM, which we will disable, then make sub-regions with the
    // appropriate attributes. 0x00000000-0x3fffffff
    MPU->RBAR = ARM_MPU_RBAR(3, 0x00000000U);    // default = no access
    MPU->RASR = ARM_MPU_RASR(1, ARM_MPU_AP_NONE, 2, 0, 0, 0, 0, ARM_MPU_REGION_SIZE_1GB);

    /* Region 4 setting I-TCM */
    // 0x00000000-0x0000ffff, Executable, cacheable
    MPU->RBAR = ARM_MPU_RBAR(4, 0x00000000U);
    MPU->RASR = ARM_MPU_RASR(0, ARM_MPU_AP_FULL, 0, 0, 1, 1, 0, ARM_MPU_REGION_SIZE_64KB);

    /* Region 5 setting D-TCM */
    // 0x20000000-0x2000ffff, Not executable, cacheable    
    MPU->RBAR = ARM_MPU_RBAR(5, 0x20000000U);
    MPU->RASR = ARM_MPU_RASR(1, ARM_MPU_AP_FULL, 0, 0, 1, 1, 0, ARM_MPU_REGION_SIZE_64KB);

    /* Region 6 setting OCRAM */
    // 0x20200000-0x2021ffff, Not executable, cacheable        
    MPU->RBAR = ARM_MPU_RBAR(6, 0x20200000U);
    MPU->RASR = ARM_MPU_RASR(1, ARM_MPU_AP_FULL, 0, 0, 1, 1, 0, ARM_MPU_REGION_SIZE_128KB);

    /* Enable MPU */
    ARM_MPU_Enable(MPU_CTRL_PRIVDEFENA_Msk);
    
    /* Enable I cache and D cache */
    SCB_EnableDCache();
    SCB_EnableICache();

}

I have no external SDRAM.

I would like somebody who understands the MPU to check for me. For example, ITCM and DTCM do not use the cache, but if I disable the cache in those regions, it does not work!

Many thanks,

Chris.

0 Kudos

1,595 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Chris Cowdery

  Seems you are using the old SDK, do you try the SDK2.8.0?

  I checked the SDK2.8.0,the ITCM, DTCM and OCRAM size is correct:

pastedImage_1.png

  Now, on your side, if you modify the related RAM size, do you still have issues or not?

  You can download the newest SDK from this link:

Welcome | MCUXpresso SDK Builder 

  You also can try the newest SDK on your side, whether after you disable the cache, you still have issues or not?

 

Best Regards,

Kerry

1,595 Views
chriscowdery
Contributor V

Hi Kerry,

 Thankyou!, that is very interesting. I see the MPU configuration has changed a lot because of Errata 1013783!

pastedImage_1.png

Does the RT1021 lock-up because of the yellow highlighted text above? And this why the default memory map must be ARM_MPU_AP_NONE?

I am going to merge in the changes from SDK2.8.0 and test.

Chris.

0 Kudos

1,595 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Chris Cowdery

  Seems related to the Arm errata 1013783-b, that's why the sdk MPU configuration also have modified the related code, just workaround speculative prefetch.

  you can test the SDK2.8.0 to check it, as I know, our SDK2.8.0 code for RT fixed a lot of bugs.

Best Regards,

Kerry

1,595 Views
chriscowdery
Contributor V

Hi Kerry,

 I believe this has fixed the problem. Impossible to prove, but the system has not crashed / locked up for 2 weeks.

Thankyou for your help.

Chris.

1,598 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Chris Cowdery

  Do you have the MIMXRT1020-EVK board?

  And can you reproduce the issue in the official board with the SDK?

Best Regards,

Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------