I was using the rt1020-evk board.I change the OCRAM size from 128KB to 64KB,but the program will enter hardFault before starting main function.
The minimum configuration of OCRAM is 64 KB according to datasheet,but i failed to change that.
So i need your help.
Thanks.
Hi,
Please make sure you are also reconfiguring IOMUXC_GPR_GPR17 register during the startup. Please check this link where my colleague gives a detailed description of how you can accomplish this.
Hope it helps!
Best regards,
Felipe
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored.
- Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
------------------------------------------------------------------------------