What does it meaning of "No muxing" in muxing options table of Reference Manual?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What does it meaning of "No muxing" in muxing options table of Reference Manual?

Jump to solution
1,230 Views
takayuki_ishii
Contributor IV

Hello community,

 

In Reference Manual of IMXRT like a IMXRT1170RM rev 1, Table 11-1. Muxing Options have "Mode" column.

What does "No muxing" mean in the "Mode" column?

 

In Reference manual of IMX6, it mean that "No muxing" pad are allocated only one signal.

It have no IOMUX and "SW_MUX_CTL_PAD_xxxxx" SW MUX Control Register.

But Reference Manual for IMXRT, many "No muxing" signals are assigned multiplex pin.

 

Best regards,

Ishii.

 

 

Tags (1)
0 Kudos
1 Solution
1,223 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) What does "No muxing" mean in the "Mode" column?
-- It means the pins will work as the corresponding function automatically once the related module is enabled.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
3 Replies
1,224 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) What does "No muxing" mean in the "Mode" column?
-- It means the pins will work as the corresponding function automatically once the related module is enabled.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
1,211 Views
takayuki_ishii
Contributor IV

Hello Jeremyzhou,

 

Thank you for your reply.

-- It means the pins will work as the corresponding function automatically once the related module is enabled.

My understanding is a  following,

If ADC1_A0 is enabled IOMUX of GPIO_AD_06 pin connect to Analog IO-ADC1_A0.

And IOMUX control registers, SW_MUX_CTL_PAD_GPIO_AD_06 and SW_PAD_CTL_PAD_GPIO_AD_06 are ignored.

Is it correct?

 

Best regards,

Ishii.

 

0 Kudos
1,202 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thanks for your reply.
1) Is it correct?
-- Yes.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos