Using xbar with timer to generate PWM signal on iMXRT1050

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Using xbar with timer to generate PWM signal on iMXRT1050

909 次查看
davidouatt08
Contributor I

Hello,

I'm using iMXRT1050 and need to generate a PWM signal on pin GPIO_B1_03, mapped to XBAR1_XBAR_INOUT17 (TMR3, TIMER_OUTPUT,0). 

Can't find any example in SDK2.5 (MCUXpresso).

Somebody already done this with iMXRT?

Regards

0 项奖励
1 回复

718 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi David OUATTARA,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
To implement the application, I think you need to do some modifications to the xbara demo.
If you have any further questions, please feel free to contact me.

Have a great day,
TIC

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励