MXRT1050 FlexSPI module have LUT which support up to 16 sequences which is equivalent to 16 Flash commands.
Many NOR Flash chips today support much more than 16 commands.
1. Is there a way to support NOR Flash devices with more than 16 flash commands ?
2. Is there a way to work with FlexSPI module without the LUT ?
Hi Ronen Avihav,
Yes, the LUT just can support up to 16 sequences, the LUT table have the size limit.
So, from my own viewpoint, I think if you think 16 sequences is not enough, after you finish the 16 sequences code, you can configure the LUT table again, just add the other command sequence, then update the LUT table and run the code.
I think the FlexSPI module need to use the LUT table to work, but more details, I will help you to check it with according department, then give you feedback.
Please waiting patiently.
Wish it helps you!
If you still have question about it, please kindly let me know.
Have a great day,
Kerry
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Thank you Kerry for the quick reply
.
if you already going to ask the R&D guys about this,
Can you please also add client request for the next chips to have more than 16 sequences ? (i.e: 32)
Waiting for your reply,
Ronen
Hi Ronen Avihav,
You can use the method which I recommend you in the above reply.
About your request, I will record it, but I don't make sure it can be accepted by the according department.
Thanks a lot for your understanding.
Have a great day,
Kerry
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hello,
I am having the same issue regarding the 16 sequence max limit. I need more than 16 sequences. I have tried to create a second LUT table to use after the Flexspi configuration, but when I try to update the LUT using FLEXSPI_UpdateLUT, it does not appear to work.
What are the complete steps for updating the LUT with different sequences? Do I need to reinitialize the Flexspi?
Hi
Here's the LUT reconfiguration from the uTasker project (I think that the NXP SDK has something similar).
The use is fnEnterLUT(pointer to the new look up table, reference to the bus - 0 for FlexSPI1 and 1 or FlexSPI2). It works for QSPI or hyper flash.
static void fnEnterLUT(const FLEXSPI_LUT_ENTRY *ptrTable, int iBus)
{
int iLUT = 0;
volatile unsigned long *ptrLUT;
iMX_FLEX_SPI *ptrFlexSPI = (iMX_FLEX_SPI *)FLEX_SPI_BLOCK;
#if FLEX_SPI_INTERFACES > 1
if (iBus != 0) {
ptrFlexSPI = (iMX_FLEX_SPI *)FLEX_SPI2_BLOCK;
}
#endif
// Update look-up table
//
while ((ptrFlexSPI->STS0 & (FLEX_SPI_STS0_ARBIDLE | FLEX_SPI_STS0_SEQIDLE)) != (FLEX_SPI_STS0_ARBIDLE | FLEX_SPI_STS0_SEQIDLE)) {} // wait until the bus is idle
ptrFlexSPI->LUTKEY = FLEX_SPI_LUTKEY_KEY;
ptrFlexSPI->LUTCR = FLEX_SPI_LUTCR_UNLOCK;
uMemset((void *)&ptrFlexSPI->LUT0, 0x00, (FLEX_SPI_LUT_ENTRIES * sizeof(unsigned long))); // ensure all non-used entries are clear
while (ptrTable[iLUT].ulReference != NOR_CMD_LUT_SEQ_IDX_END_OF_TABLE) {
ptrLUT = &ptrFlexSPI->LUT0;
ptrLUT += ((ptrTable[iLUT].ulReference & 0x0f) * 4); // move to the LUT entry
if (*ptrLUT != 0) {
_EXCEPTION("Overlapping LUT indexes being used!!!!");
}
*ptrLUT++ = ptrTable[iLUT].ulEntrySequence[0]; // enter the sequence(s)
*ptrLUT = ptrTable[iLUT].ulEntrySequence[1];
#if defined BOOT_HYPER_FLASH
*(++ptrLUT) = ptrTable[iLUT].ulEntrySequence[2];
*(++ptrLUT) = ptrTable[iLUT].ulEntrySequence[3];
#endif
iLUT++;
}
ptrFlexSPI->LUTKEY = FLEX_SPI_LUTKEY_KEY;
ptrFlexSPI->LUTCR = FLEX_SPI_LUTCR_LOCK;
ptrFlexSPI->MCR0 |= FLEX_SPI_MCR0_SWRESET; // perform a reset of the module
_WAIT_REGISTER_TRUE(ptrFlexSPI->MCR0, FLEX_SPI_MCR0_SWRESET); // wait for reset to complete
}
Note that a SW reset is made to the module before using the new table.
Regards
Mark
[uTasker project developer for Kinetis and i.MX RT]
Contact me by personal message or on the uTasker web site to discuss professional training, solutions to problems or rapid product development requirements
For professionals searching for faster, problem-free Kinetis and i.MX RT 10xx developments the uTasker project holds the key