What are the differences between M7 in iMXRT1060 and M7 in iMX8MP...

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What are the differences between M7 in iMXRT1060 and M7 in iMX8MP...

Jump to solution
1,237 Views
EdSutter
Senior Contributor II

I've done a few projects with the iMXRT1060, and I'm now about to embark on an iMX8MP project.  Is there any chart that compares the M7 on the iMXRT1060 to the M7 on the iMX8?  Yea, I'll be digging into the datasheets, but figured I'd post the question while I'm doing that...

I assume things like exceptions, cache, TCM & MPU are identical (true?).

What about peripherals?  Since both devices are NXP, it would be nice to hear that some of them (UART, I2C, SPI etc...) were the same...??? 

Labels (2)
0 Kudos
Reply
1 Solution
1,201 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @EdSutter ,

    As I know, the M7 in the RT1060 and the IMX8MP is similar.

    There no chart that compares these two chip, as one is MCU, another is processor.

     To the IMX8MP M7 memory map and IP, you can refer to the RM, 

   https://www.nxp.com/webapp/Download?colCode=IMX8MPRM

chapter 2.3 Cortex-M7 Memory Map

and the related IP chapter.

As I know, peripherals is also similar.

  If you have more question about the IMX8MP, you can create the issues in the i.mx processor area:

https://community.nxp.com/t5/i-MX-Processors/bd-p/imx-processors

 

Wish it helps you!

Best Regards,

Kerry

   

View solution in original post

0 Kudos
Reply
1 Reply
1,202 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @EdSutter ,

    As I know, the M7 in the RT1060 and the IMX8MP is similar.

    There no chart that compares these two chip, as one is MCU, another is processor.

     To the IMX8MP M7 memory map and IP, you can refer to the RM, 

   https://www.nxp.com/webapp/Download?colCode=IMX8MPRM

chapter 2.3 Cortex-M7 Memory Map

and the related IP chapter.

As I know, peripherals is also similar.

  If you have more question about the IMX8MP, you can create the issues in the i.mx processor area:

https://community.nxp.com/t5/i-MX-Processors/bd-p/imx-processors

 

Wish it helps you!

Best Regards,

Kerry

   

0 Kudos
Reply