USB Audio device class (i.MXRT1050) doesn't work on Windows 10

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB Audio device class (i.MXRT1050) doesn't work on Windows 10

2,598 Views
dav1
Contributor V

Hi,

The USB Audio device class example (usb speaker) for the i.MXRT1050 doesn't work on Windows 10.

it plays for 0.5sec then stops. Any chance we can see an update soon? Preferably incl. UAC2.0.

ps. works great on macOS.

Team NXP,

  • can we get in touch with the people that wrote this Audio Device class driver?
  • is there a list of OS'es this has been tested against? (linux, mac, iOS, windows, android)!?
  • is there a git-repository for the driver-code so where the development/patches so far can be followed!?
Labels (1)
5 Replies

2,106 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi,

Have you tried the example avoiding using USB HUBs and direct connection to computer’s USB ports instead?

Regarding driver availability, they are released on each SDK version release, and their changes are summarized on the Release Notes document of each release.

In case of requiring a custom implementation of the USB Audio driver, you could consider NXP Professional Services.

For more information regarding this, please refer to the following link:

https://www.nxp.com/support/support/nxp-professional-services:PROFESSIONAL-SERVICE


Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,106 Views
dav1
Contributor V

Hi, Any updates to this in the latest SDK_2.6.1?

not sure where to find the release-notes / history for a specific driver.

0 Kudos
Reply

2,106 Views
dav1
Contributor V

Hi Carlos,

1. Sounds like this could be in the USB core itself then, probably not handling "non multi-tt hubs correctly" or USB split transactions. Can you please file a bug-report to get this resolved?

2. What is the purpose of these drivers, demo or production use? Is there a list available on how these have been tested, what os'es etc!?

Thanks David

0 Kudos
Reply

2,106 Views
dav1
Contributor V

ping. any plans to continue work, making the audio host/device driver for RT-series more stable?

0 Kudos
Reply

2,106 Views
dav1
Contributor V

ping again

0 Kudos
Reply