Hi,
Regarding MIMXRT1170-EVK, let me ask.
I downloaded SDK using CMSIS-DAP with EWARM on verC board and could check the function.
For exp sample)
C:\XXXXX\boards\evkmimxrt1170\driver_examples\mu
And after getting new version C2 of MIMXRT1170-EVK, I cannot check the function
due to CoreSight error without reading IDCODE. It means no SWD access.
According to this result, I think that new action is needed.
Can you comment something to this phenomena?
For exp)
I would like to understand if it is necessary for users to update CMSIS-DAP driver.
Regards,
Koichi
解決済! 解決策の投稿を見る。
Hi,
I summarized a document written how to debug using i-jet provided by IAR.
Please see attached file.
Regards,
Koichi
Hi Gustavo,
Thank you for your comment.
I got it.
Regards,
Koichi
Hello Koichi,
From version C to C1 and C2 there was no layout change, but there were some BOM updates.
From C to C1:
1.Change C346 from 100nF to 100pF.
2.Change R368 from DNP 10K ohm to populate 100K ohm.
3.DNP R136 and default to use SD CD/DAT3 for card detection
From C1 to C2:
I hope that this information helps!
Regards,
Gustavo