The EMC & EMI of a two-layer RT1020 circuit board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

The EMC & EMI of a two-layer RT1020 circuit board

774件の閲覧回数
614678489
Contributor I

In our products, some components and interconnectors are very sensitive to the Electro-Magnetic Radiation or the Electro-Magnetic Field,  how is the EMC & EMI of a two-layer RT1020 board, do I need to prepare a Faraday Cage for our sensitive components and interconnectors ?

Thanks a lot.

ラベル(1)
0 件の賞賛
1 返信

683件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Fun

Hardware Development Guide for the MIMXRT1020 Processor gives general layout

recommendations for emc issues.
https://www.nxp.com/docs/en/nxp/user-guides/MIMXRT1020HDUG.pdf

However also one can use any available methods for reducing emc sensitivity on

custom board.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛