RT1064 内部4M的Flash是否可以模拟EEPROM用

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT1064 内部4M的Flash是否可以模拟EEPROM用

1,336 Views
1914795885
Contributor II

你好:

      我想用RT1064 内部4M的Flash保存一些简单的传感器数据,但是看了一下2.4版本的SDK,并没有发现类似的例子。除了保存用户代码的部分,其余部分是否可以作为数据存储使用?如果可以,是否有相关的例程呢?

谢谢!

0 Kudos
Reply
1 Reply

1,047 Views
victorjimenez
NXP TechSupport
NXP TechSupport

Hello,

Please check the following community thread (link).


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply