The message you are trying to access is permanently deleted.
Hi,
I have a MIMRT1020-EVK board.
Following the AN12238 i.MX RT Flashloader Use Case (https://www.nxp.com/docs/en/nxp/application-notes/AN12238.pdf ) . Though this document is written for 1050, I assume the steps would be the same for 1020.
Get error- "Error: Initial ping failure: No response received for ping command."
Notice that the USB did not re-enumerate to VID/PID 0x15A2/0x0073. We remain at 1FC9/130.
Attached is the console log.
Repeated the above with usb (-u) option same issue.
What am I missing here?
regards,
Ashish
Is there a resolution for this problem? Do you have source code for mfgtool.exe that can be provided to retrofit it into Linux mode of operation?
Hello,
I think the option "get-property" under item 5 should be applied to the USB port.
The flashloader uses the USB.
Regards,
Yuri.
I tested USB-HID port, it seems the board doesn't jump to the new USB-HID(vid="15A2" pid="0073), so I don't use command, I use the mfgtool.exe in the flashloader folder, the board jump successfully, then I use
"blhost.exe -u get-property 1" get the correct messgae, you can try it
Yes but we cannot use mfgtool.exe in field since its a windows utility.
We would like to support OTA firmware update where the firmware would be downloaded on to master board (Android/Linux) and applied on the various sub-systems over uart.
Looking at the MfgTool logs and the ucl2.xml it seems the mfgtool.exe is calling sdphost and blhost to load the ivt_flashloader and program the flash. We would like to update the firmware using the same either via scripts or writing our own application.
Is source available for the tools?
Was the question about retrofitting mfgtool to Linux ever answered? Is there source code available to do this?
Thanks.