Hi,
I'm using NXP IMX RT 1062 and i need to get the same PWM signal (controllable through the FlexPWM peripheral) out of the uC on these 2 pins GPIO_SD_B0_04 and GPIO_EMC_09.
Unfortunately it is not possible to associate the same FlexPWM submodule to both pins, and i need the signals to be synchronous.
I was wondering if it is possible to achieve a similar result driving one pin as FLEXPWM output and the other as duplicated output using XBAR matrix without CPU intervention.
I have no experience on XBAR peripheral, add all examples that i have found on SDK are not about FlexPWM and GPIO.
Is this possible? any examples?
Thank you very much!
Best Regards
Emanuele
Yes, this is possible! See my post here: https://community.nxp.com/t5/i-MX-RT/imxrt1052-connect-pwm-out-to-xbar-out-pin-by-xbar/m-p/1724065/h.... After routing the PWM signal to the XBAR, you can then configure the needed pin(s) as XBAR outputs (using IOMUXC_GPR->GPR6) and then connect them to FLEXPWMn_PWMx_OUT_TRIGy in the XBAR. That should duplicate the XBAR signal on those pin(s).