Hi there,
I am currently developing with the i.MX RT1050 Evaluation Kit and developing the GUI.
This is the emWin example provided by the SDK, emwin_gui_demo. It runs perfectly on a 4.3-inch LCD which the resolution is 480x272.
However, when I switch it to a 7-inch LCD, the problem occurs as shown in the attached image.
The whole GUI is mirrored and duplicated. Besides, there is a black region left and the GUI could not fill it.
Is there any method that I could try to solve it?
Hi Alex Wong ,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
I think I need to know more information about the phenomenon, so whether you can introduce what modification did about the emwin_gui_demo, in further, I'll appreciate a lot if you can share the schematic of the 7-inch LCD.
Looking forward to your reply.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi Jeremy,
Actually I didn't modify much on emwin_gui_demo. Only int k = LCD_SetSize(800,480); is added into emwin_gui_demo.c for changing the physical size and send k to the terminal to check whether it runs successfuly or not.
Also, the loopDivider is set to 39 and post divider is set to 4 for the LCD.
Thank you.
Alex