Mimxrt117x SDK 12.0 example

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Mimxrt117x SDK 12.0 example

738 Views
akash-lawande
Contributor II

Hello
I am using mimxrt117x evk kit with wifi test example(sdio) from sdk 12.0 .while using in debugging mode i am getting Closed Telnet Session msg randomly then debugging sessions closed completely.

Can you guide me why i am getting this error??

0 Kudos
3 Replies

696 Views
estephania_mart
NXP TechSupport
NXP TechSupport

Hello,

 

Could you please also help us with the module you are using with the example ? Also , could you please also help me confirm that you are using UART and not semihosting ? Also which version of the MCUXPresso IDE are you using ? Did you made some modification to the code example ?

 

Regards

0 Kudos

694 Views
akash-lawande
Contributor II

Hello thanks for Reply

my problem is solved  

718 Views
jay_heng
NXP Employee
NXP Employee

Are you using MCUXpresso IDE project?The default build is Xip Build, the stability may be affected by flashloader, you can switch to RAM build as below:

Capture.PNG

0 Kudos