MfgTool for RT1170 EVK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MfgTool for RT1170 EVK

Jump to solution
1,068 Views
namsu_mun
Contributor III
Hi, I am looking for MfgTool of RT1170 EVK. If not available, please tell me how to modify cfg.ini and ucl2.xml of other model, such as rt1106X. Thanks Namsu
Tags (1)
0 Kudos
1 Solution
1,060 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
There's a MfgTool for RT1170 EVK and you can find it resides in the SDK library (~\middleware\mcu-boot\bin\Tools).
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

3 Replies
1,061 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
There's a MfgTool for RT1170 EVK and you can find it resides in the SDK library (~\middleware\mcu-boot\bin\Tools).
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

1,042 Views
namsu_mun
Contributor III

Hi Jeremy,

I am testing mfgtool-rel of "SDK_2.9.1_MIMXRT1170-EVK\middleware\mcu-boot\bin\Tools" with rt1170evk. but found some problem as follows;

ModuleID[2] LevelID[10]: ExecuteCommand--Blhost[WndIndex:0], Body is load-image "Profiles\MXRT117X\OS Firmware\ivt_flashloader.bin"
ModuleID[2] LevelID[10]: PortMgrDlg(0)--Path=\\.\hid#vid_1fc9&pid_013d#6&30f3aaaa&0&0000#{4d1e55b2-f16f-11cf-88cb-001111000030}
ModuleID[2] LevelID[1]: Jumping to Flashloader. [WndIndex:0]
ModuleID[2] LevelID[10]: CmdOperation[0], current command executed failed, so SetEvent(hDevCanDeleteEvent)

Please refer to attached log file. And the RT1170 SDK has no "blhost", so just copy it from FLASHLOADER-RT1064-1.0.

Thank you,

Namsu

0 Kudos
1,027 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thanks for your reply.
Please try the blhost.exe in the attachment.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos