I use NXP Imx RT1170 EVK board and NXP’s own ide, MCU Xpresso. I have downloaded their latest version for now (03 Feb 2024). I had a project about GUI, there are some texts and images and buttons.
I wanted to import lvgl v9 after released. I can see the same screen on my lcd but I could not get successful touch. I think I have a problem about indev, I share some code pieces and screens here.
Previous version v8.3.11
void lv_port_indev_init(void)
{
static lv_indev_drv_t indev_drv;
DEMO_InitTouch();
lv_indev_drv_init(&indev_drv);
indev_drv.type = LV_INDEV_TYPE_POINTER;
indev_drv.read_cb = DEMO_ReadTouch;
lv_indev_drv_register(&indev_drv);
}
new version v9.0.0 written by me
void lv_port_indev_init(void)
{
lv_indev_t * indev = lv_indev_create();
DEMO_InitTouch();
lv_indev_set_type(indev,LV_INDEV_TYPE_POINTER);
lv_indev_set_read_cb(indev,DEMO_ReadTouch);
lv_indev_set_display(indev,disp);
}
Video is here : https://veed.io/view/a6df6215-cb30-4c41-9a26-10a940bda5f8
解決済! 解決策の投稿を見る。
Hi thanks for support. I thought I have a problem about indev but I was wrong. My problem was about lv_display_t .
I have written below code
memset(s_frameBuffer, 0, sizeof(s_frameBuffer));
lv_display_t * disp = lv_display_create(DEMO_BUFFER_WIDTH, DEMO_BUFFER_HEIGHT);
lv_display_set_flush_cb(disp, (void *)DEMO_FlushDisplay);
lv_display_set_buffers(disp, s_frameBuffer[0], s_frameBuffer[1], DEMO_BUFFER_WIDTH*DEMO_BUFFER_HEIGHT*DEMO_BUFFER_BYTE_PER_PIXEL, LV_DISPLAY_RENDER_MODE_PARTIAL);
Then I have changed just render_mode as below and now touch capability is okay.
lv_display_set_buffers(disp, s_frameBuffer[0], s_frameBuffer[1], DEMO_BUFFER_WIDTH*DEMO_BUFFER_HEIGHT*DEMO_BUFFER_BYTE_PER_PIXEL, LV_DISPLAY_RENDER_MODE_DIRECT);
Now I can see my gui designs on the lcd and when I touch objects I see an expected effects.
Hi @frozen ,
Thank you for your interest in the NXP MIMXRT product, I would like to provide service for you.
I already help you to check with our internal side, LVGL V9 is not supported now.
We highly recommend you use the following LVGL version which is supported by the GUI Guider:
Then, if you meet any issues, just kindly let us know.
Best Regards,
Kerry
Hi @kerryzhou ,
Thanks for your support. I have to use v9, that's why I have to insist on not using Gui Guider with lvgl v8.3.5.
Hi @frozen ,
I already check internally, the V9+SDK still in the progress internally, as V9 have a lot of difference with V8. So, until now, SDK support with V9 still not avaiable, thanks.
Best Regards,
Kerry
Hi thanks for support. I thought I have a problem about indev but I was wrong. My problem was about lv_display_t .
I have written below code
memset(s_frameBuffer, 0, sizeof(s_frameBuffer));
lv_display_t * disp = lv_display_create(DEMO_BUFFER_WIDTH, DEMO_BUFFER_HEIGHT);
lv_display_set_flush_cb(disp, (void *)DEMO_FlushDisplay);
lv_display_set_buffers(disp, s_frameBuffer[0], s_frameBuffer[1], DEMO_BUFFER_WIDTH*DEMO_BUFFER_HEIGHT*DEMO_BUFFER_BYTE_PER_PIXEL, LV_DISPLAY_RENDER_MODE_PARTIAL);
Then I have changed just render_mode as below and now touch capability is okay.
lv_display_set_buffers(disp, s_frameBuffer[0], s_frameBuffer[1], DEMO_BUFFER_WIDTH*DEMO_BUFFER_HEIGHT*DEMO_BUFFER_BYTE_PER_PIXEL, LV_DISPLAY_RENDER_MODE_DIRECT);
Now I can see my gui designs on the lcd and when I touch objects I see an expected effects.