Hello,
As title, I have the IMXRT1060 devboard (just the one), trying to get CAN-FD working, and it point blank refuses to.
Got it hooked up to a PCAN device (rather then a 2nd EVK for the transfer example), and can verify the hardware is wired up correctly as I get the one-shot massage through for the CAN example ok.
But when I reconfigure the PCAN for the default 1/2Mbps and try the CAN-FD example, I get nothing.
Further, if I stop the debugger, it's trapped in the while (!txComplete) suggesting that the transfer hasn't actually occurred at all, and not just a bus speed issue.
It seems I'm the only one with this issue, as googling shows no useful results, hence asking here.
Suggestions?
Thanks.
已解决! 转到解答。
Aaaand... The issue is fixed elsewhere on this forum!
Summary: FD ISO is disabled by default and needs to be manually enabled by editing the driver file.
Aaaand... The issue is fixed elsewhere on this forum!
Summary: FD ISO is disabled by default and needs to be manually enabled by editing the driver file.