IMXRT1060-EVK CAN-FD transfer example not working, CAN is.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMXRT1060-EVK CAN-FD transfer example not working, CAN is.

Jump to solution
1,124 Views
p_shep
Contributor IV

Hello,

As title, I have the IMXRT1060 devboard (just the one), trying to get CAN-FD working, and it point blank refuses to.

Got it hooked up to a PCAN device (rather then a 2nd EVK for the transfer example), and can verify the hardware is wired up correctly as I get the one-shot massage through for the CAN example ok.

But when I reconfigure the PCAN for the default 1/2Mbps and try the CAN-FD example, I get nothing.

Further, if I stop the debugger, it's trapped in the while (!txComplete) suggesting that the transfer hasn't actually occurred at all, and not just a bus speed issue.

It seems I'm the only one with this issue, as googling shows no useful results, hence asking here.

 

Suggestions?

Thanks.

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
1,120 Views
p_shep
Contributor IV

Aaaand... The issue is fixed elsewhere on this forum!

https://community.nxp.com/t5/i-MX-RT/CAN-FD-using-MIMXRT1064-EVK-and-PCAN-View-PC-software/m-p/10348...

Summary: FD ISO is disabled by default and needs to be manually enabled by editing the driver file.

 

View solution in original post

0 Kudos
Reply
1 Reply
1,121 Views
p_shep
Contributor IV

Aaaand... The issue is fixed elsewhere on this forum!

https://community.nxp.com/t5/i-MX-RT/CAN-FD-using-MIMXRT1064-EVK-and-PCAN-View-PC-software/m-p/10348...

Summary: FD ISO is disabled by default and needs to be manually enabled by editing the driver file.

 

0 Kudos
Reply