IMXRT1024 LPUART Transmit Output and TXD Pin

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMXRT1024 LPUART Transmit Output and TXD Pin

ソリューションへジャンプ
651件の閲覧回数
Lukas_Frank
Senior Contributor I

Hi all,

 

Q.1. What is the difference between transmitter output and TXD Pin? Isn't already the output of the transmitter TXD Pin? Where is the transmitter output in figure 44-1?

Lukas_Frank_1-1625656871384.png

Q.2. Whhy we use TXINV and RXINV? Why we need to inverse/reverse polarity of transmitted data output?

 

Thanks and Regards.

 

0 件の賞賛
1 解決策
639件の閲覧回数
victorjimenez
NXP TechSupport
NXP TechSupport

Hello, 

Q.1. What is the difference between transmitter output and TXD Pin? Isn't already the output of the transmitter TXD Pin? Where is the transmitter output in figure 44-1?

Transmitter output and TXD pin are the same things. 

Q.2. Whhy we use TXINV and RXINV? Why we need to inverse/reverse polarity of transmitted data output?

You don't need to invert these signals, however, the module gives you the option to do so in case your working environment demands it. This is mentioned in the LPUART Control Register and LPUART Status Register. 

Regards,
Victor

元の投稿で解決策を見る

0 件の賞賛
1 返信
640件の閲覧回数
victorjimenez
NXP TechSupport
NXP TechSupport

Hello, 

Q.1. What is the difference between transmitter output and TXD Pin? Isn't already the output of the transmitter TXD Pin? Where is the transmitter output in figure 44-1?

Transmitter output and TXD pin are the same things. 

Q.2. Whhy we use TXINV and RXINV? Why we need to inverse/reverse polarity of transmitted data output?

You don't need to invert these signals, however, the module gives you the option to do so in case your working environment demands it. This is mentioned in the LPUART Control Register and LPUART Status Register. 

Regards,
Victor

0 件の賞賛