IMX RT 1024: FlexSPI DQS pin mandatory to float?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX RT 1024: FlexSPI DQS pin mandatory to float?

228 Views
bp1979
Senior Contributor I

We have a question regarding the FlexSPI DQS pin for the 1024 to run flash on a frequency of 133 MHz.

In this answer we read that it is "highly recommended" to leave the DQS pin floating.

Can you please explain:

- should it only float when connected to external flash? Thus, if connected to the internal flash in a 1024 "second die", must DQS then still float?

- what if we don't, what is the risk?

0 Kudos
1 Reply

216 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello
I hope you are well.

It is suggested to float DQS so you can use the flash at max specified speed. If using 1024 which has a SoC flash it is still suggested to float that pin.
If you don’t float the pin then you will find a limit in operating frequency.

Best regards,
Omar

0 Kudos