How to flash an .hex file into the i.MX RT1020 EVK?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to flash an .hex file into the i.MX RT1020 EVK?

1,245件の閲覧回数
arimendes
Contributor III

Hi,

 What tools can I use to load a .hex file into the i.MX RT1020 EV and run the code?

0 件の賞賛
2 返答(返信)

1,178件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
To provide the fastest possible support, I'd highly recommend you use the NXP-MCUBootUtility which is a GUI tool specially designed for NXP MCU secure boot. Its features correspond to the BootROM function in NXP MCU.
Please give a try.
https://github.com/JayHeng/NXP-MCUBootUtility

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛

1,162件の閲覧回数
pholden
Contributor II

Is there a flash programming tool that runs on Linux?

0 件の賞賛