How to flash an .hex file into the i.MX RT1020 EVK?

cancel
Showing results for 
Search instead for 
Did you mean: 

How to flash an .hex file into the i.MX RT1020 EVK?

651 Views
arimendes
Contributor III

Hi,

 What tools can I use to load a .hex file into the i.MX RT1020 EV and run the code?

0 Kudos
2 Replies

584 Views
jeremyzhou
NXP TechSupport
NXP TechSupport

Hi

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
To provide the fastest possible support, I'd highly recommend you use the NXP-MCUBootUtility which is a GUI tool specially designed for NXP MCU secure boot. Its features correspond to the BootROM function in NXP MCU.
Please give a try.
https://github.com/JayHeng/NXP-MCUBootUtility

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos

568 Views
pholden
Contributor II

Is there a flash programming tool that runs on Linux?

0 Kudos