Datasheets of MiMXRT1175AVP8A(144 pin), MiMXRT1175AVJ8A(196 pin)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Datasheets of MiMXRT1175AVP8A(144 pin), MiMXRT1175AVJ8A(196 pin)

Jump to solution
577 Views
venkat7
Contributor I

Hi,

    I need details of what peripherals available in small form package of  of imxrt1170, they are 

MiMXRT1175AVP8A(144 pin) - 10 x 10 mm

MiMXRT1175AVJ8A(196 pin)  - 12 x 12 mm.

I need what are the peripherals available in the above two packages. I googled them but they are not available.

Please send datasheets/manuals of above both part numbers.

Thank you,

K.Venkatarao.

0 Kudos
Reply
1 Solution
559 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thanks for your reply.
1) Are they not in production yet?
-- Yes, you can think so.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
3 Replies
570 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
The above two packages are not available, so I'm not assured of they will not contain the peripherals versus MIMXRT1175AVM8A.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply
567 Views
venkat7
Contributor I

Thank you for your reply.

But as per "i.MX RT1170 Crossover  Processors Data Sheet for Automotive Products".

144, 196 pin configuration available. see below pic, are they not in production yet?

144 pin package RT1175.png

0 Kudos
Reply
560 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thanks for your reply.
1) Are they not in production yet?
-- Yes, you can think so.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply