DCDC converter does not produce 1.2V

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DCDC converter does not produce 1.2V

Jump to solution
818 Views
msaliharslan
Contributor III

Hi MX-RT1052 MCU on a custom board does not produce 1.2V. We measure about 1.13 V from where it should be 1.2 V. What are the possible causes of this? Also, does the processor operate with 1.13V?

Edit: Our DCDC_IN_Q pin connected to 3.3 V via PCB trace with 8 mOhm resistance, is this a problem?

Edit 2: Supplying 1.2V from an external power source  we observed that no current is supplied to the processor.

Labels (1)
0 Kudos
1 Solution
797 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
To provide the fastest possible support, I'd highly recommend you to refer to MIMXRT1050 to adjust your custom board to check the DCDC_OUT can output an expected voltage.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
1 Reply
798 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
To provide the fastest possible support, I'd highly recommend you to refer to MIMXRT1050 to adjust your custom board to check the DCDC_OUT can output an expected voltage.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos