Can I use external Static RAM with i.MXRT1050? I need more Static RAM with battery backup

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can I use external Static RAM with i.MXRT1050? I need more Static RAM with battery backup

1,317件の閲覧回数
Soos
Contributor III

Is it possible to use external static RAM with iMXRT1050 ?

I need more battery backed-up RAM for our application.

タグ(1)
2 返答(返信)

1,211件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

 

  The SEMC of the RT1050 supports devices with general purpose SRAM-like
interface.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,211件の閲覧回数
Soos
Contributor III

OK Thanks

I will use SEMC_CSX0 as CS for my Static RAM.