Can I use a MIMXRT1064 as a drop in replacement for a 1062 with no software changes

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can I use a MIMXRT1064 as a drop in replacement for a 1062 with no software changes

Jump to solution
826 Views
caleb
Contributor III

Hello, 

Is it possible to use the 1064 as a drop-in replacement on a board that uses a 1062, with no software/linkage changes, and just boot from the already extant external flash chip?

Is there any gotcha that I need to know about? 

Thanks, 

-caleb 

0 Kudos
1 Solution
820 Views
mjbcswitzerland
Specialist V

Hi Caleb

The i.MX RT 1062 boots from external QSPI at 0x60000000.

The i.MX RT 1064 boots from its internal QSPI at 0x70000000. It is not possible to boot from the external one, even though it would be at 0x60000000.

Regards

Mark

 

View solution in original post

2 Replies
815 Views
caleb
Contributor III

Thanks again Mark!

 

0 Kudos
821 Views
mjbcswitzerland
Specialist V

Hi Caleb

The i.MX RT 1062 boots from external QSPI at 0x60000000.

The i.MX RT 1064 boots from its internal QSPI at 0x70000000. It is not possible to boot from the external one, even though it would be at 0x60000000.

Regards

Mark