AR1335 camera sensor driver

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

AR1335 camera sensor driver

8,375 Views
fmabrouk
Contributor III

@kerryzhou 

I am wondering if you have used this camera sensor: AR1335 with any of your NXP MCUs. If so please share with me the driver source code.

Regards,

Farid

0 Kudos
24 Replies

5,123 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi fmabrouk,

  Thanks for your information.

   Please keep patient, I will check more details about your code, and check with our internal CSI expert.

  After I get any valuable information, I will let you know ASAP.

  Please give me more time, thanks so much!

 

Best Regards,

kerry

0 Kudos

5,088 Views
fmabrouk
Contributor III

@kerryzhou

i hope you are doing well! I just want to follow up with you and see if you got any updates for my issue. 

Again I need help configure the CSI driver so that I can capture the 10 bits raw data for each output pixel data. After capturing the data I can use my own software to convert data to a RGB 888 format. 

Thank you! 

0 Kudos

4,990 Views
fmabrouk
Contributor III

Any feedback to my issue from other members of the forum or NXP team. I’m really out of time and need to sort this out! Please help if you can. 

 

0 Kudos

5,008 Views
fmabrouk
Contributor III

Hello Kerry,

One more thing I want to let you know about is that the output format of the camera sensor is: RAW10 ( 10 bits) and in the current nXP CSI/camera driver I dont see this format supported. I see only these ones:

/*! @brief Pixel format definition. */
typedef enum _video_pixel_format
{
/* RGB */
kVIDEO_PixelFormatXRGB8888 = FSL_VIDEO_FOURCC('X', 'R', '2', '4'), /*!< 32-bit XRGB8888. */
kVIDEO_PixelFormatRGBX8888 = FSL_VIDEO_FOURCC('R', 'X', '2', '4'), /*!< 32-bit RGBX8888. */
kVIDEO_PixelFormatXBGR8888 = FSL_VIDEO_FOURCC('X', 'B', '2', '4'), /*!< 32-bit XBGR8888. */
kVIDEO_PixelFormatBGRX8888 = FSL_VIDEO_FOURCC('B', 'X', '2', '4'), /*!< 32-bit BGRX8888. */

kVIDEO_PixelFormatRGB888 = FSL_VIDEO_FOURCC('R', 'G', '2', '4'), /*!< 24-bit RGB888. */
kVIDEO_PixelFormatBGR888 = FSL_VIDEO_FOURCC('B', 'G', '2', '4'), /*!< 24-bit BGR888. */

kVIDEO_PixelFormatRGB565 = FSL_VIDEO_FOURCC('R', 'G', '1', '6'), /*!< 16-bit RGB565. */
kVIDEO_PixelFormatBGR565 = FSL_VIDEO_FOURCC('B', 'G', '1', '6'), /*!< 16-bit BGR565. */

kVIDEO_PixelFormatXRGB1555 = FSL_VIDEO_FOURCC('X', 'R', '1', '5'), /*!< 16-bit XRGB1555. */
kVIDEO_PixelFormatRGBX5551 = FSL_VIDEO_FOURCC('R', 'X', '1', '5'), /*!< 16-bit RGBX5551. */
kVIDEO_PixelFormatXBGR1555 = FSL_VIDEO_FOURCC('X', 'B', '1', '5'), /*!< 16-bit XBGR1555. */
kVIDEO_PixelFormatBGRX5551 = FSL_VIDEO_FOURCC('B', 'X', '1', '5'), /*!< 16-bit BGRX5551. */

kVIDEO_PixelFormatXRGB4444 = FSL_VIDEO_FOURCC('X', 'R', '1', '2'), /*!< 16-bit XRGB4444. */
kVIDEO_PixelFormatRGBX4444 = FSL_VIDEO_FOURCC('R', 'X', '1', '2'), /*!< 16-bit RGBX4444. */
kVIDEO_PixelFormatXBGR4444 = FSL_VIDEO_FOURCC('X', 'B', '1', '2'), /*!< 16-bit XBGR4444. */
kVIDEO_PixelFormatBGRX4444 = FSL_VIDEO_FOURCC('B', 'X', '1', '2'), /*!< 16-bit BGRX4444. */

/* YUV. */
kVIDEO_PixelFormatYUYV = FSL_VIDEO_FOURCC('Y', 'U', 'Y', 'V'), /*!< YUV422, Y-U-Y-V. */
kVIDEO_PixelFormatYVYU = FSL_VIDEO_FOURCC('Y', 'V', 'Y', 'U'), /*!< YUV422, Y-V-Y-U. */
kVIDEO_PixelFormatUYVY = FSL_VIDEO_FOURCC('U', 'Y', 'V', 'Y'), /*!< YUV422, U-Y-V-Y. */
kVIDEO_PixelFormatVYUY = FSL_VIDEO_FOURCC('V', 'Y', 'U', 'Y'), /*!< YUV422, V-Y-U-Y. */

kVIDEO_PixelFormatXYUV = FSL_VIDEO_FOURCC('X', 'Y', 'U', 'V'), /*!< YUV444, X-Y-U-V. */
kVIDEO_PixelFormatXYVU = FSL_VIDEO_FOURCC('X', 'Y', 'V', 'U'), /*!< YUV444, X-Y-V-U. */
} video_pixel_format_t;

 

Can Raw10 be converted to RGB888 in the application code?

I attached some data sheets for your reference.

0 Kudos