ADC+DMA

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ADC+DMA

3,423 Views
leonidshigris
Contributor III

Hello,

My evaluation board: NXP IMXRT1050-EVKB.

SDK_2.6.0_EVKB-IMXRT1050

There is only sdk example:  adc_etc_hardware_trigger_conv

I try to understand, how can I config ADC with DMA ?

I can't find any documents that explain this type of configuration.

Also no examples refer to this issue.

Best Regards,

Leon.

Labels (4)
0 Kudos
Reply
4 Replies

2,971 Views
leonidshigris
Contributor III

Hi jeremyzhou Employee,

I see the next example : https://community.nxp.com/docs/DOC-335320

Very similar to my request.

One of my questions,

1. SIM->SOPT7 |= 0x8EU; 

This type of register doesn't exist in IMXRT1050.

How I link between ADC and QTMR ?

Best Regards,

Leon.

0 Kudos
Reply

2,971 Views
leonidshigris
Contributor III

Hi jeremyzhou Employee

Thank you for this info,

But  I expect to see the real example as part of IMXRT1050 SDK.

Is it expected to add such an example and when?

Best Regards,

 

Leon.

0 Kudos
Reply

2,972 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Leonid Shigris,

Thanks for your reply.
1) Is it expected to add such an example and when?
-- As I know, there's no plan to add such example in the SDK in recent.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

2,972 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Leonid Shigris,

Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
Yes, there's no similar demo as you want in the SDK library, but I've attached two application notes which describe how to combine the ADC and DMA, even these two notes are base on Kinetis MCU, however, they still can inspire you, as RT MCU and Kinetis share the ADC and DMA IPs.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply