26MHz external crystal for RT600

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

26MHz external crystal for RT600

688件の閲覧回数
mark_wu
Contributor II

Hello,

In i.MX RT600 datasheet show the crystal oscillator operating range 1MHz to 25MHz,

but in the description of clock sources, external clock input pin(50MHz Max),

so can I use a 26MHz external crystal for RT600?

Thanks.

pastedImage_1.png

pastedImage_2.png

ラベル(1)
2 返答(返信)

595件の閲覧回数
fangfang
NXP TechSupport
NXP TechSupport

Hello,

>> so can I use a 26MHz external crystal for RT600?

No, crystal oscillator operating range 1MHz to 25MHz, SO the customer can not use a 26MHz external crystal for RT600.

External clock input (CLKIN function from a pin, selected by IOCON) is not for the crystal.

Have a nice day.

Best regards

595件の閲覧回数
mark_wu
Contributor II

Thank you

0 件の賞賛