Source code: https://github.com/JayHeng/NXP-MCUBootUtility 【v1.3.0】 Features: > 1. Can generate .sb file by actions in efuse operation utility window > 支持生成仅含自定义efuse烧写操作(在efuse operation windows里指定)的.sb格式文件 Improvements: > 1. HAB signed mode should not appliable for FlexSPI/SEMC NOR device Non-XIP boot with RT1020/1015 ROM > HAB签名模式在i.MXRT1020/1015下应不支持从FlexSPI NOR/SEMC NOR启动设备中Non-XIP启动 > 2. HAB encrypted mode should not appliable for FlexSPI/SEMC NOR device boot with RT1020/1015 ROM > HAB加密模式在i.MXRT1020/1015下应不支持从FlexSPI NOR/SEMC NOR启动设备中启动 > 3. Multiple .sb files(all, flash, efuse) should be generated if there is efuse operation in all-in-one action > 当All-In-One操作中包含efuse烧写操作时,会生成3个.sb文件(全部操作、仅flash操作、仅efuse操作) > 4. Can generate .sb file without board connection when boot device type is NOR > 当启动设备是NOR型Flash时,可以不用连接板子直接生成.sb文件 > 5. Automatic image readback can be disabled to save operation time > 一键操作下的自动程序回读可以被禁掉,用以节省操作时间 > 6. The text of language option in menu bar should be static and easy understanding > 菜单栏里的语言选项标签应该是静态且易于理解的(中英双语同时显示) Bugfixes: > 1. Cannot generate bootable image when original image (hex/bin) size is larger than 64KB > 当输入的源image文件格式为hex或者bin且其大小超过64KB时,生成可启动程序会失败 > 2. Cannot download large image file (eg 6.8MB) in some case > 当输入的源image文件非常大时(比如6.8MB),下载可能会超时失败 > 3. There is language switch issue with some dynamic labels > 当切换显示语言时,有一些控件标签(如Connect按钮)不能实时更新 > 4. Some led demos of RT1050 EVKB board are invalid > /apps目录下RT1050 EVKB板子的一些LED demo是无效的 【v1.4.0】 Features: > 1. Support for loading bootable image into uSDHC SD/eMMC boot device > 支持下载Bootable image进主动启动设备 - uSDHC接口SD/eMMC卡 > 2. Provide friendly way to view and set mixed eFuse fields > 支持更直观友好的方式去查看/设置某些混合功能的eFuse区域 Improvements: > 1. Set default FlexSPI NOR device to align with NXP EVK boards > 默认FlexSPI NOR device应与恩智浦官方EVK板卡相匹配 > 2. Enable real-time gauge for Flash Programmer actions > 为通用Flash编程器里的操作添加实时进度条显示
View full article