NXP Launches the GHz MCU Era with the i.MX RT1170

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NXP Launches the GHz MCU Era with the i.MX RT1170

NXP Launches the GHz MCU Era with the i.MX RT1170

The newly announced i.MX RT1170 is a dual-core Arm® Cortex®-M based crossover MCU that breaks the gigahertz (GHz) barrier and accelerates advanced Machine Learning (ML) applications at the edge.  Built using advanced 28nm FD-SOI technology for lower active and static power requirements, i.MX RT1170 MCU family integrates a GHz Arm Cortex-M7 and power-efficient Cortex-M4, advanced 2D vector graphics, together with NXP’s signature EdgeLock security solution.  The i.MX RT1170 delivers a total CoreMark score of 6468 and address the growing performance needs of edge computing for industrial, Internet-of-Things (IoT) and automotive applications

コメント

Is there a timeline on preliminary documentation (datasheets, RMs) for designers?

評価なし
バージョン履歴
最終更新日:
‎10-02-2019 10:35 AM
更新者: