usb driver for RT1172 missing

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

usb driver for RT1172 missing

Jump to solution
2,591 Views
ingdb
Contributor III

Hello all,

I am trying to use USB on a RT1172 but I can't generate a SDK with USB drivers included. 

ingdb_0-1690526015058.png

The RT1176 processor is working. 

ingdb_0-1690526246420.png

 

Is this a SDK bug? Did anyone every used the SDK driver for a RT1172 processor?

best regards

Matthias

Tags (1)
0 Kudos
Reply
1 Solution
2,179 Views
diego_charles
NXP TechSupport
NXP TechSupport

Hi @ingdb 

Just to continue with the follow up.

The reason of this error is the manifest file. Our team will do the necesary changes to add USB references, as some where missing.

All the best,

Diego

 

 

 

View solution in original post

0 Kudos
Reply
14 Replies
2,290 Views
diego_charles
NXP TechSupport
NXP TechSupport

Hi @ingdb 

Thanks a lot for your patience, and again, for reporting this bug.

We further reproduced this issue internally with the SDK 2.14.0 

Our MCUXpresso IDE and SDK team is now aware of this bug. Given the fact that we just released SDK 2.14 and IDE 11.8. We will need to wait a bit to get this error corrected in the SDK, I pressume a minor release. 

To workarround this situation, currently, I have some suggestions:

A  For development use the RT1172 SDK 2.13.1 that I shared to you by your salesforce ticket. 

B to use SDK 2.14.0 : Create a project from the RT1172 SDK 2.13.1 drivers including the USB middleware. Create your SDK 2.14.0 project without the drivers. Unzip the SDK 2.14.0 somewhere else, and manually copy and paste drivers, files and adrresses.

We will check the manifest file from the SDK. Maybe this is the reason of the issue. Our Investigation is going on. As soon I get more news I will update you.

Thank you for your understanding. 

Diego

0 Kudos
Reply
2,180 Views
diego_charles
NXP TechSupport
NXP TechSupport

Hi @ingdb 

Just to continue with the follow up.

The reason of this error is the manifest file. Our team will do the necesary changes to add USB references, as some where missing.

All the best,

Diego

 

 

 

0 Kudos
Reply
2,341 Views
diego_charles
NXP TechSupport
NXP TechSupport

Hi @ingdb 

Thanks a lot for your patience. 

I replicated this issue with the Plug-in SDK ( SDK 2.14 and IDE v11.8). In turns out that the SDK 2.13 that you can get from mcuxpresso SDK builder did  not show this issue on my side. 

diego_charles_0-1691442142315.pngdiego_charles_1-1691442152991.png

I am already reporting this internally. As we can not attach the SDKs directly in  the community, due to their size,  I am going to attach the SDK version that did not presented this issue in the internal case that you created. 

I will get back to you  with more news on this. 

Best regards, 

Diego

 

 

0 Kudos
Reply
2,326 Views
ingdb
Contributor III

Hello Diego,

the SDK version you created is working for me, but it's not related to the version. When generating a SDK based on 13.1 in my dashboard that's not working for me.

 

best regards

Matthias

0 Kudos
Reply
2,317 Views
diego_charles
NXP TechSupport
NXP TechSupport

Hi Mattias, 

Thanks for lettting me know. 

Please attach your SDK 2.13.1 to the files section of the case. 

Again, thanks a lot for the patience. 

Diego

Edit: typo

0 Kudos
Reply
2,544 Views
ingdb
Contributor III

Hi Diego,

 

thanks for your help. A SDK with all middleware activated didn't help. But I am going to test with the new IDE next week. But I'd be curious, could you send me your SDK?

 

best regards

Matthias

0 Kudos
Reply
2,498 Views
diego_charles
NXP TechSupport
NXP TechSupport

Hi Mattias, 

MCUXpresso v11.8 is already available, could you give a try? (please build SDK 2.14)

Anyway, this is the share link to RT1172 SDK 2.13 I generated https://mcuxpresso.nxp.com/download/2ccf22b6f09a437a989583c2c37b2fe8

All the best, 

Diego

0 Kudos
Reply
2,490 Views
ingdb
Contributor III

Hi Diego,

I tested with MCUExpresso v11.8 and SDK 2.14, same effect.

This link is not working for me:

https://mcuxpresso.nxp.com/download/2ccf22b6f09a437a989583c2c37b2fe8

Error message: Alert:  You do not have authorized access for this archive

 

and another strange effect when selecting the SDK of the MIMXRT1172 but with the MIMXRT1176 processor the USB drivers are available. But when selecting the MIMXRT1172 SDK  with the MIMXRT1172 processor I don't see the USB driver. 

Best regards 

Matthias

0 Kudos
Reply
2,488 Views
ingdb
Contributor III

but I see the relevant files in the SDK, it looks as if it's a problem of the MCUExpresso?

ingdb_0-1690972331110.png

 

0 Kudos
Reply
2,480 Views
ingdb
Contributor III

we tested on 4 PC, everywhere the same behavior.

0 Kudos
Reply
2,468 Views
diego_charles
NXP TechSupport
NXP TechSupport

Hi @ingdb 

Thanks for your response. 

Interesting, would you please confirm to me your OS version? I did not see this on Windows 11 as well. 

The SDK that I used can not be attached due to its file size. 

Best regards,

Diego

0 Kudos
Reply
2,453 Views
ingdb
Contributor III

Hello Diego,

We tested on windows 10 and windows 11

Best regards

Matthias 

0 Kudos
Reply
2,421 Views
ingdb
Contributor III

Hi Diego,

That's a nasty bug, I see two options, we merge the USB driver in our project manually or we use a different processor. We created a support case at NXP, maybe we get some help.

It's a pity, IMHO the NXP software flow is superior to the ST flow, but the ST tools are more stable.

best regards

Matthias

 

0 Kudos
Reply
2,576 Views
diego_charles
NXP TechSupport
NXP TechSupport

Hi @ingdb 

I hope you are doing well. 

I checked with the below  SDK and IDE versions. 

diego_charles_0-1690571387121.png

diego_charles_1-1690571395041.png

But I could not reproduce the issue you are showing. See below image. 

diego_charles_2-1690571450053.png

I used Windows 10 OS too. When I build the SDK I included all middleware. If this is not your case please detail the above to check further. 

btw, SDK 2.14.0 is already released , and MCUXpresso IDE 11.8.0 is coming problaby next week. So maybe you can give a try with this latest SW too.

Best regards, 

Diego

 

 

0 Kudos
Reply