Hi echo zeng,
非常感谢使用NXP产品,很高兴为你提供技术支持!
请介绍一下你的测试过程和分享烧录失败的错误提示截图。
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
jeremyzhou,你好!
bin文件大于16M时:用usb(烧写bin)和iar flashloader(导入out)烧写失败,iar flashloader烧写后,无法进入debug模式,重新开机后无法启动。
iar flashlodaer烧写失败log:download-debug-log-1.zip
bin文件小于16M时:usb和flashloadder烧写和启动都正常。
另外,根据IS25LP512M datasheet,访问大于16M的空间需要设置bank选择位或者设置地址为32bit。bootrom是否可以设置或支持32bit qspi访问地址?flash地址截图见附件.
多谢 !
Hi echo zeng,
感谢回复。
你是指你测试SDK软件包中的bootloader_examples过程中,发现flashloader工程只能成功烧录小于(16M)的application image,超过其大小限制的,就会烧录失败,是这样吗?
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
1,是指用“IAR安装目录下的FlashIMXRT1050_EVK_FlexSPI.out”烧写小于16Mok,大于16M会出现校验错误。
2,如果修改了 “FlashIMXRT1050_EVK_FlexSPI.out”,如何配置xip "flexspi_mem_config_t memConfig"?
启动时需要将flash切换到32bit地址模式,以下参数如何配置:
“uint8_t configModeType[3]; //!< [0x01d-0x01f] Configure Mode Type, similar as deviceModeTpe”
“flexspi_lut_seq_t
configCmdSeqs[3]; //!< [0x020-0x02b] Sequence info for Device Configuration command, similar as deviceModeSeq”
“ uint32_t configCmdArgs[3]; //!< [0x030-0x03b] Arguments/Parameters for device Configuration commands”
谢谢!
Hi echo zeng,
1) 是指用“IAR安装目录下的FlashIMXRT1050_EVK_FlexSPI.out”烧写小于16Mok,大于16M会出现校验错误。
-- 建议先调整Flash Loader大小,使其与IS25LP512M适应。
2)4-byte address 可以支持启动设置。
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi echo zeng,
感谢回复。
1)flash地址与你截图的一致(我这里多了个--setQE)
-- 你可以把你的截图贴出来我看看,还有再分享一下烧录失败的错误提示截图。
2)可以通过.boot_hdr.conf:flexspi_nor_config_t来配置么?
-- 不可以。
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
jerremyzhou,你好!
1)flash地址与你截图的一致(我这里多了个--setQE)
-- 你可以把你的截图贴出来我看看,还有再分享一下烧录失败的错误提示截图。
通过修改flashloader,已经可以烧写64Mflash,勾选了verify选项,下载完成后不再有错误提示。
2)可以通过.boot_hdr.conf:flexspi_nor_config_t来配置么?
-- 不可以。
为免问题描述不清晰,我再说明一下:64M flash默认寄存器是24位地址,必须修改一个叫bank的寄存器,将其改为支持32位地址 。如果要支持xip启动的话,a,需要bootrom通过boot_hdr.conf中配置的lut sequence来设置这个寄存器使能flash支持32位地址。b,在boot_hdr.conf的lut表中让flexspi接口使能4b(FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0xEB, RADDR_SDR, FLEXSPI_4PAD, 0x20/*0x18*/)/*0x18=24bit address, 0x20=32bit address*/)(iar flashloader里面是通过SetLUT32b来实现的)
以上实现方式确实不可行么 ?必须用BOOT_CFG[2:0]来实现?
谢谢!
Hi echo zeng,
感谢你的回复。
Q1) 好的,就是说现在是可以成功下载了哦,但是代码没有启动上来对吗?
Q2) 在查看FlexSPI Memory Configuration结构后,没有可以用于执行以下command sequence的设置。
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
jeremyzhou,你好!
1),修改iar flashloader后可以下载,可以跑起来,但跑起来与16M flash对比,非常(动态图形界面)卡,是否是因为没有进入QPI模式?
2),我留意到:FlexSPI Memory Configuration,有几个参数:是否可以利用起来:
.deviceModeCfgEnable = true,
.deviceModeType = 1,//Quad Enable command
.deviceModeSeq.seqNum = 1,
.deviceModeSeq.seqId = 4,
.deviceModeArg = 0x000040,
这是用于设置QE使能的是sequence。
但还有一组参数:看起来与上述功能一致,可能也是可以利用的,但我不太清楚 怎么使用:
uint8_t configModeType[3];
flexspi_lut_seq_t configCmdSeqs[3];
uint32_t configCmdArgs[3];
以上两组参数,bootrom是如何执行的?谁先谁后?
configModeType:“Configure Mode Type, similar as deviceModeTpe”,而deviceModeType的注释是“Specify the configuration command type:Quad Enable, DPI/QPI/OPI switch ! Generic configuration, etc.“这个参数如何取值?
能否帮忙说明一下,多谢!
Hi echo zeng,
请先发给flexspi_nor_config_t的配置,我先帮你看看。
这样讨论起来比较有效率一点。
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi echo zeng,
感谢回复。
在查看了附件后,我发现你是想通过如下设置,但是正如参考手册222页提到的,LUT表内的command sequence顺序是已经定义好了的,你不能随意更改。
建议是使能Customized LUT sequence,自己添加Fig 1所示对应的command sequence。
.deviceModeSeq.seqNum = 1,
.deviceModeSeq.seqId = 4,
.deviceModeArg = 0x000040,
Fig 1
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
uint8_t lutCustomSeqEnable; //!< [0x047-0x047] LUT customization Enable, it is required if the program/erase cannot
//! be done using 1 LUT sequence, currently, only applicable to HyperFLASH,目前hyperFlash才能用,qspi flash呢?
你说的使能“Customized LUT sequence”与上面的冲突了,麻烦确认。
谢谢!
Hi echo zeng,
感谢回复。
参考手册没有备注这个信息,但是保守起见我会向AE team求证一下后再回复你。
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
...so?
How is it possible to send 0xB7 command during XIP initialization? Someone could help understanding how deviceModeSeq and configCmdSeqs are intended to be used for such purpose, if so? Please?