imxrt Ethernet reception not working

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imxrt Ethernet reception not working

640件の閲覧回数
ancymuhammed
Contributor III

We are using iMXRT1176 interfaced to PHY chip KSZ8081RNB. Ethernet page schematics attached.

The below is the pin details connected to imxrt. ENET_CRS_DV is connected to the pin GPIO_DISP_B2_08 and ENET_INT is connected to GPIO_AD_12.

 
 

ancymuhammed_2-1668689238299.png

We build around 30 boards. We are facing reception not working in three boards. One board works after replacing the RJ45 connector with new one and one board works after replacing the microcontroller. We had checked all the waveforms between micro & PHY and PHY & connector. It looks same as the working board.  While checking the loop back action, we found that digital loopback is failed, and analog loopback is working fine. Could you please look into this.

 

0 件の賞賛
返信
0 返答(返信)