Hi fellas,
I'v created a new cpp based project in for iMX RT1064 for lwip+freeRTOS. For comparision, I've used tcp_echo project, which is based on c.
I've succedded till "Initializing PHY" . After that the chip ID for PHYKSZ8081(32/0x22) is not able to read by PHY_KSZ8081_READ @ fsl_phyksz8081.c file.
I hope the main issues lies in ENET_ReadSMIData @ fsl_enet.c file, as previous funtion's return is SUCEESS ony (i.e.).ENET_MDIOWaitTransferOver
Let me come whre the actual problem might me...
I've configured the pins & clocks as per the c project in mu cpp. Is there anything else should be modified w.r.t cpp or specificlly for ETHERNET configurations?
PS : Exmaple, FreeRTOSConfig.h file's max priority has been set to 5 --> while, lwip_rx has priority has 8. One changed, it worked. Similarly, any config files that I should check w.r.t ETH
已解决! 转到解答。
Hi all,
Issues has been resolved. Reason is I've created a multiple threads - in which ETH_RST & ETH_INT has been used for onboard led.
They were toggling - which interrupted the whole process.
Hi all,
Issues has been resolved. Reason is I've created a multiple threads - in which ETH_RST & ETH_INT has been used for onboard led.
They were toggling - which interrupted the whole process.